The General table in the Carrier n node enables you to turn the Imported carrier on and off, and select a saved channel configuration.
The Baseband parameters for the Imported Waveform are described in Baseband (Imported Waveform).
After an external waveform is loaded:
1. General |
---|
Double-click or use the drop-down menu to enable or disable the carrier.
Selects the name of the waveform file to be loaded into the software.
Displays the Source Sampling Rate of the waveform. This parameter is read only and automatically set by the software.
The value is determined from the waveform currently loaded into memory. This parameter is read only and automatically set by the software.
Displays the required waveform license of the waveform currently loaded into memory. This parameter is not editable.